CSV file samples
Create CSV files to add multiple devices at once. The following files are samples of files that can be used for some of the various communication protocols.
For more information, defining multiple devices, see Define multiple devices using a CSV file.
DNP3 for Serial and Ethernet
                                            
                                        
IEC104.2
                                            
                                        
IEC61850