TGML templates
TGML templates are available for graphics devices, such as Micrologic MTZ, PowerTag, and HDPM. The required template can be copied to your project and the generic pop-up link can be updated using Graphics Editor.
By default, all TGML templates are located in:
..\Program Files (x86)\Schneider Electric\Power Operation\v2022\Applications\Services\Platform Server\PLS_Include\TGML\Templates
Your project does not have all of the template files by default, as they can overload the project. It is recommended that you copy the TGML template you need for your project, and then save it to the following location:
..\ProgramData\Schneider Electric\Power Operation\v2022\User\PLS_Include\TGML\Templates
Prerequisites:
- Your project has a Templates folder set up in the following location:
..\ProgramData\Schneider Electric\Power Operation\v2022\User\PLS_Include\TGML
- Save the desired device template folder from
..\Program Files (x86)\Schneider Electric\Power Operation\v2022\Applications\Services\Platform Server\PLS_Include\TGML\Templates
to the following location under ProgramData:..\ProgramData\Schneider Electric\Power Operation\v2022\User\PLS_Include\TGML\Templates
NOTE: Create the Templates folder if it is not available in the previous location.
NOTE: For improved pop-up or link navigation, it is recommended that you maintain the default folder structure for your source and destination hierarchy. Any change in folder structure or file name requires you to reconfigure the link property in the TGML graphic.
For more information, see Navigating between TGML templates.