TGML Components: <Component>
The Components element is a container element (similar to Group) which defines a reusable group of elements.
Top and Left of Component specifies the position of the component in the parent coordinate system. Component itself establishes a new coordinate system for the contained elements, which means that the upper left corner of Component is the origin (0,0) for the contained elements.
Width and Height specifies the "viewport" (size on screen) of the component. ContentWidth and ContentHeight specify the "viewbox", which is the boundary of the contained elements. If the viewport is different from the viewbox, a scale transformation is applied by the TGML implementation (similar to Stretch="Fill"). For more information, see TGML Document Type Element and Metadata. In other words, resizing a Component has the effect of scaling the content of the Component.
The Clip attribute specifies if the renderer shall clip elements that exceed (are drawn outside) the specified viewbox or not.
When a Component includes Bind or Link elements, the Name of Component will prefix the exposed bind names ("MyComponent.MyBind").
For more information, see TGML Components.
| Attribute | Type | Description |
|---|---|---|
|
Clip |
Bool |
Specifies if the content shall be clipped or not. |
|
ContentHeight |
Double |
Specifies the viewbox height (height of the content). |
|
ContentWidth |
Double |
Specifies the viewbox width (width of the content). |
|
Height |
Double |
The viewport height of the component (height on screen). |
|
Left |
Double |
The x coordinate of the component's upper left corner. |
|
Opacity |
Double |
A value between 0.0 (transparent) and 1.0 (opaque). |
| Top | Double |
The y coordinate of the components upper left corner. |
| Visibility | Visibility |
Specifies if the element shall be visible or not. |
| Width | Double |
The viewport width of the component (width on screen). |
Example:
<TGML>
<Rectangle Left="0.0" Top="55" Width="30" Height="30" Fill="#FFOO00" Stroke="#FF0000" />
<Polyline Points="30.0,65.0 60.0,5.0 90.0,35.0" Stroke="#FF0000" StrokeWidth="2.0"/>
<Component Left="150.0" Top="20.0" Width="50.0" Height="50.0" ContentWidth="91" ContentHeight="86">
<Rectangle Left="0.0" Top="55" Width="30" Height="30" Fill="#FF0000" Stroke="#FF0000" />
<Polyline Points="30.0,65.0 60.0,5.0 90.0,35.0" Stroke="#FFQOOO" StrokeWidth="2.0"/>
</Component>
</TGML>
Example on screen: