Adding a thermal monitoring Device to a Power Operation project

To add a thermal monitoring Device to a Power Operation project using the profile you created in Configuring a thermal monitoring device profile:

  1. Open the I/O Device Manager.
  2. In the I/O Device Manager, confirm the correct project is selected in the Project Name drop down.
  3. Select Manage a Single Device to open the I/O Device Manager Wizard.
  4. Select Create one I/O Device and select Next.
  5. In Choose Profile, select the thermal monitoring device profile you created and select Next.
  6. Enter an Equipment name and I/O device name.
  7. Select your communications method, Modbus/TCP or Modbus/RTU Via Gateway.
  8. Enter the SMD communication settings.
  9. Enter a custom port name or keep the generated default, and select Next.
  10. Select Finish.

    NOTE: If you are adding multiple SMD devices, select Add / Remove / Update more equipment and repeat steps 1-10 for each.