Configuring SMS Text Notification
Short Message Service (SMS) sends a notification as a text message when an alarm occurs in a configured notification, or when you select the SMS Notifications Test button.
Prerequisites:
- A modem that accepts a standard SIM card and connects to the computer using a USB cable (the connection is a serial connection). Compatible modems include: MultiTech MTD-H5, or MultiTech MTC-H5-B03.
- A SIM card from a carrier that lets you send automated messages and large numbers of text messages at one time.
- The modem COM port. For more information, see Determining modem COM ports.
Moxa OnCell G3111 is not supported.
NOTE: Certain carriers restrict how you can use their services.
To configure SMS text notifications:
- In Power Operation Runtime, open Notifications Settings.
- Select Settings and Diagnostics, and then select SMS Setup.
- Change the Alarm Server from the drop-down list, if required.
NOTE: If multiple alarm servers are set up, the first one in the list is automatically selected.
- Enter the modem COM port.
- (Optional) Set the other SMS values.
Refer to the following table for a description of the SMS settings:
- Select Save and Close. The Save Configuration screen displays.
- To save the configuration across all the alarm servers, select Save.