Determining modem COM ports
To determine the modem COM port:
- Open Windows Device Manager.
- Expand Ports (COM & LPT).
- Take note of the COM port value. You will need to enter this value in Notifications Settings. See Configuring SMS Text Notification.
- Configure the COM Port with the following values:
The port is listed beside the modem in brackets.
| COM Port Settings | Values |
|---|---|
| Bits per second | 115200 |
| Data bits | 8 |
| Stop bits | 1 |
| Parity | None |
| Flow control | None |