Devices

Use Profile Studio to configure Power Operation in accordance with IEC 61850-standard engineering workflows.

Use Profile Editor to create device types and device profiles outside of the IEC 61850-standard engineering workflow.