Redundant systems configuration
NOTE: This section assumes that Power Operation project and Primary Server are configured.
To configure redundant systems you must copy and export project files from the Primary Server to the Secondary Server.
See the following topics for detailed information on configuring and updating a redundant system:
Topic | Description |
---|---|
Configure the Power Operation Primary Server | Lists the procedures to copy and export that will be subsequently imported on the Secondary Server. |
Configure the Power Operation Secondary Server | Lists the procedures to import the Primary Server files onto the Secondary Server. |
Updating on redundant systems | Information on how to make changes on a redundant system without interruptions to the system. |