Configure the Power Operation Primary Server

NOTE: This section assumes that Power Operation project and Primary Server are configured.

Complete the following configuration tasks on the Primary Server:

The files you back up and export on the Primary Server will subsequently be copied or imported into the Secondary Server.