Snippets Pane
Use the Graphics Editor Snippets pane to manage function categories:
NOTE: To get a description of a snippet, right-click the snippet in the list, and then select Properties.
| Component | Description |
|---|---|
| Basic Functions | This category contains standard functions delivered with the program.
For more information, see the Snippets Overview section. |
| Global Bind | This category contains global bind snippets delivered with the program. For more information, see the Snippets Overview section. |
| Snippets Global Graphic Scripts | This category contains global graphic scripts delivered with the program. For more information, see the Snippets Overview section. |
| My Snippets | This category is where you save customized functions that you want to reuse in the future. For more information, see the Snippets Overview section. |