Read, Export, Print, and Edit Basic Reports

After you create a basic report, you can:

  • Change its appearance (Page Setup)
  • Print it
  • Change its view: HTML or PDF
  • Scroll to the beginning, previous page, next page, or last page
  • Export it to a variety of formats
  • Email it

The following table describes the toolbar options:

Option Description
Parameters/Report Toggle between viewing the parameters (setup) page and the report
Prent/Child reports Not currently used.
Hide/Show Not currently used.
Page Setup Click this link to open the Page setup window, where you can determine paper size, and page orientation and margins.
Print

Click this link to print the report.

NOTE: For best formatting of the report, you should export to PDF, and then print.

Print Preview In HTML mode, click this link to view the print output.
Viewer Mode You can view in HTML or PDF mode. Select the mode, then click Viewer Mode to change the view.
Viewer Mode Set () Click to confirm the choice of viewer mode.

Pagination

Click the left and right arrows to page backward and forward in the report. Or type the page number you want to see.
Select a format For exporting, choose the printable format (not HTML) that you want.
Export () See instructions below for exporting a report.
Email () Click this link, and then enter the requested information. Click Send. For other ways to email reports, see Email basic reports

Exporting a Basic Report

Before you can print a basic report, you must export it into one of the following printable formats:

  • PDF
  • Web Archive
  • Word Document
  • XML File
  • XLS Document

To export a report:

  1. While viewing the report, select a printable format, then click Export.
  2. Type the location at which you want to save the file.
  3. Set any other properties you wish.
  4. Click Export.
  5. NOTE: To export a large quantity of data, consider using Tabular Report Exports.

Edit the Basic Report appearance

With the report displayed, you can:

  • Change the paper size
  • Change the paper source
  • Change the page orientation
  • Change the page margins
  • Change the number of pages per sheet
  • Add a watermark