Tabular Report Exports

Use Tabular Report Export to generate a CSV file of your system's historical data. Tabular Report Exports can include multiple devices and multiple topics. A Tabular Report Export contains a table with timestamped data points on each selected device and topic within the period selected.

NOTE: A Tabular Report Export can include a maximum of 60 days, 72 devices, and 16 topics per report.

To create a Tabular Report Export:

  1. Browse to the Tabular Report Export in the reporting web application. When prompted, enter your Power Operation user account information. Select Login.
  2. Enter the following:
    1. Title – Enter a name for your report.
    2. In the Reporting Period, select a date range for the report.
    3. Devices – Select the names of the devices for the report.
    4. Topics – Select the topics to be included.
    5. If you require two different sampling interval trends for the same variable tag, you must create a duplicate of the existing variable tag and confirm that:

      • Tag Name, ItemName, and Comment are unique for each tag.
      • Trend tag names should be the same as the variable tag name.

    6. Select Generate Report Export.
    7. On the Report Export List page, a table of reports generated for export is shown. When the Ready column displays True for your desired report, select Download. The exported CSV file will download as a ZIP file.

If a Tabular Report Export takes a long time to generate and you are logged out, or if you want to view previously exported reports, do the following:

  1. Browse to the Tabular Report Export in the reporting web application. When prompted, enter your Power Operation user account information. Select Login.
  2. Select View Report Exports to view the Report Export List page. Reports are ready to be downloaded when the Ready column displays True.

For more information about reports, see Read, Export, Print, and Edit Basic Reports.