Integration with EcoStruxure™ Building Operation (EBO) - Planning

The integration of PME with EBO – hereafter referred to as PME/EBO Integration solution – is an engineered solution that embeds features of EcoStruxure™ Power Monitoring Expert (PME) into EcoStruxure™ Building Operation (Building Operation).

The PME/EBO Integration solution provides access to PME Dashboards, Reports, Diagrams, alarm and real-time data through Building Operation, for a seamless user experience.

PME/EBO Integration solution is intended for large buildings, such as high-rise commercial office buildings, shopping malls, and university campuses. It provides easy to understand energy information for building managers with limited electrical systems knowledge.

 

This integration planning section includes the following topics:

NOTE: The deployment of the PME/EBO Integration solution requires application engineering expertise in installing and configuring EBO and PME.