Other IT considerations

Internet Information Services (IIS) .NET Trust Level

The .NET Trust Level for PME web applications and Default Web Site must be set to Full (internal), in IIS Manager. See IIS Application Pools for a list of PME web (ASP.NET) applications.

PME Server name limitations

The computer name for the PME server must have 15 characters or less, and use only letters, numbers or hyphens.

NOTE: The computer name must not be changed after the PME software is installed. If the computer name is changed after the install, the software ceases to function correctly. If that occurs, contact Technical Support for assistance.

Display resolution

The minimum display resolution for PME user interfaces is 1280 x 960 pixels.