Licensing process
The licensing process is different for new systems, system upgrades, and system migrations. The following shows the high-level process for each. For further information, see the resources provided in Licensing resources.
New system licensing
The following flowchart shows the high-level licensing process for new PME systems:
System upgrade licensing
The following flowchart shows the high-level licensing process for PME system upgrades:
(*) PME systems must be upgraded using a services plan with software assurance.
System migration licensing
The following flowchart shows the high-level licensing process for moving a PME system to a new server, or reinstalling it on the same server after the operating system has been reinstalled:
See System migration and license returns for more details.
Related topics:
- Licensing overview
- Licensing process
- Licensing tools
- Important notes on licensing
- Operating System licensing
- SQL Server Licensing
- Other software licensing
- Licensing configuration
For reference information see: