Other software licensing

PME can be used with a number of third party, add-on applications. These applications can be integrated with PME or can be used standalone. Check the licensing requirements of these applications before using them with PME.

Third party software licenses for add-on applications are not included in the PME license. Schneider Electric does not resell third party add-on licenses.

Examples of third-party add-on applications include:

  • Microsoft Office
  • Virtual Machine software
  • Third party OPC server/client software
  • Virus and malware detection and application control software

Related topics:

For reference information see: