Creating new measurements
You can use Manual Data Editor to create new, custom measurements in PME. These measurements are available anywhere in the software.
To create a new measurement:
- In Manual Data Editor, click Load New Data to open the Load Data dialog box.
NOTE: Load Data opens automatically when you start Manual Data Editor.
- In Load Data, click Create new Measurement to open the Create new Measurement dialog box.
NOTE: Check the list of available measurements to see if one exists for your application before creating a new measurement.
- In Create new Measurement, enter the relevant information for the new measurement.
- Click Create to add the new measurement to the system.
- (Optional) Repeat steps 2-4 to add additional measurements.
- Close Manual Data Editor.
For information on how to use the Manual Data Editor , see:
- Editing existing logged measurement data
- Adding manually collected measurement data
- Viewing previous change details
- Reverting previous data edits
- Creating new measurements
For reference information see: