Software Modules
Software modules combine different software features and capabilities to create a specific set of deliverables. Software modules are designed around a particular application. Examples of software modules include the Power Quality Performance Module, the Energy Analysis Reports Module, and the Breaker Performance Module.
This section provides configuration information for the software modules in PME.
Use the links in the following table to find the module you are looking for:
| Module | Application |
|---|---|
| Backup Power Module configuration |
Generator and Uninterruptible Power Supply (UPS) performance monitoring and reporting, including battery health. |
| Breaker Performance Module configuration |
Circuit breaker aging and breaker settings monitoring. |
| Capacity Management Module configuration |
Generator and Uninterruptible Power Supply (UPS) capacity monitoring and reporting. Includes transformer and UPS loss monitoring. |
| Energy Analysis Dashboard Module configuration |
Gadgets for identifying consumption patterns and anomalies and for comparing different consumers over time. |
| Energy Analysis Reports Module configuration |
Reports for energy consumption monitoring and modeling, including energy usage by process area or by product output. |
| Energy Billing Module configuration |
Energy-based billing and reporting, including consumption monitoring and reporting at the branch circuit level. |
| Event Notification Module configuration |
Notifications of power system events via email, SMS, or SNMP. |
| Insulation Monitoring Module configuration |
Monitoring for isolated power systems, such as the ones found in hospital operating rooms. |
| Power Quality Performance Module configuration |
Analysis of power quality events and disturbances and their impact on the monitored system. |