Backup Power Module configuration
NOTE: This module requires a separate license. See Licensing for more information.
The Backup Power Module provides generator and Uninterruptible Power Supply (UPS) monitoring and reporting. It reports on generator and UPS performance and battery health.
The Generator Test EPSS Report can be configured to conform to the requirements for an Emergency Power Supply System (EPSS) test, including automatic transfer switches (ATS). For example, the report shows the transfer time of the lead ATS and indicates whether the transfer time passes or does not pass the test requirements. See Emergency Power Supply Systems for more information on EPSS.
The following reports, diagrams, and tools are part of this module:
| Type | Reports | Diagrams | Tools | 
| Generator Performance | Generator Activity Generator Battery Health Generator Test EPSS Generator Load Summary | EPSS Diagrams | Generator Performance Configuration(*) | 
| UPS Performance | UPS Auto Test | UPS Auto Test diagrams | UPS Configuration | 
| UPS Battery Health | n/a | n/a | 
(*) The Generator Performance Configuration tool includes the Run History, which is a record of the generator run activities.
To use the reports and diagrams in this module, the module must be configured, and the measurement data must be available as historical data logs in the database.
For configuration information on the different component types, see:
- Configure Generator Activity Report
- Configure Generator Battery Health Report/Export
- Configure Generator Test EPSS
- Configure Generator Load Summary Report
- Configure UPS Performance
Related topics:
Backup Power Module topics
- Backup Power Module design
- Backup Power Module configuration
- Backup Power Module operation
Other Software Modules
- Breaker Performance Module configuration
- Capacity Management Module configuration
- Energy Analysis Dashboard Module configuration
- Energy Analysis Reports Module configuration
- Energy Billing Module configuration
- Event Notification Module configuration
- Insulation Monitoring Module configuration
- Power Quality Performance Module configuration