Configuring a network diagram
Before you can view the network diagram in the Diagrams application, you must generate a network diagram (network.dgm
) in Vista. The Diagrams application uses the network diagram generated in Vista for display in the browser. The network diagram is automatically added to the Diagram Library, all you need to do is generate the network diagram in Vista, save it in the default location, and then restart the Diagrams application.
Note that the Vista component is installed with Power Monitoring Expert on a primary server or Engineering Client.
To generate a default network diagram in Vista:
- Start Vista.
- Click File > Generate network diagram.
- Click File > Save.
Related topics:
- Configuring Devices diagrams
- Configuring a Network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagrams registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see Diagrams.