Diagrams registry settings
notice
IRREVERSIBLE OPERATING SYSTEM DAMAGE OR DATA CORRUPTION
Before making any changes, back up your Windows Registry in a network folder or other remote location.
Failure to follow these instructions can result in irreparable damage to the operating system of the computer and all existing data.
NOTE: Registry edits must be performed only by qualified and experienced personnel.
The registry keys are in HKEY_LOCAL_MACHINE\SOFTWARE\Wow6432Node\
The following table lists the default Diagrams registry entries and settings.
The following table lists the optional registry entries you can set for custom functionality. Modifying system registry keys without the required knowledge or experience in these procedures can damage the computer's operating system and all existing data.
| Optional Entries | Default Settings | Description |
|---|---|---|
| NetworkDiagram | x-pml:/diagrams/ud/ network.dgm |
This value specifies the network diagram to display as the homepage for Diagrams. The value can be a relative path, such as the default setting, or it can be an absolute file path (e.g.: D:\customdiagrams\ud\networkB.dgm). |
| QueryTimeout | See description. | This value determines how long Diagrams waits for the results of a query to return from the database before timing out. If this registry entry is not created or no QueryTimeout value is specified, Diagrams times out after 60 seconds. |
| This optional registry entry is useful if you know that a query will take more than 60 seconds to return its results and you do not want Diagrams to time out before then. Specify a value that gives you enough time to get your query results. |
Related topics:
- Configuring Devices diagrams
- Configuring a network diagram
- Creating custom diagrams
- Set default options for a diagram
- Set Diagrams control options
- Diagram Library
- Diagram registry settings
- Configuring a custom network diagram for direct browser access
- Configuring Power Quality Performance diagrams
- Configuring Power Quality Performance diagrams for multiple sites
For information on how to use Diagrams, see