System Language

Use these system localization settings to select the language, region, and currency symbol. The setting for Region determines date, time, number, and currency formats.

NOTE: Your personal localization settings overrule the system localization settings for your user account. By default, your personal localization settings are the same as the system localization settings. See System and personal localization settings for details on the behavior of these settings.

NOTE: The system localization settings also apply to the diagrams displayed in the Vista application.

To change any of the system localization settings:

  1. Select the options you want from the drop-down lists.
  2. Click Save to apply the changed settings.