System and personal localization settings
NOTE: The language settings in System Language and Personal Preferences determine the language the web applications are displayed in.
By default, the localization settings in Personal Preferences are the same as the ones in System Language. Changes to the settings in System Language are automatically copied to the Personal Preferences settings as long as the Personal Preferences settings have never been customized. After you customized the Personal Preferences localization settings once, they will no longer change when the System Language settings are changed.
NOTE: Your personal localization settings overrule the system localization settings for your user account.
Example 1: Language settings in Personal Preferences follow System Language if they have never been customized.
| Condition | Language Settings | Comments |
|---|---|---|
| Default | System Language: English Personal Preferences: English |
This is assuming the software was installed as an English system. |
| Change System Language to French | System Language: French Personal Preferences: French |
The Personal Preferences language settings follow the System Language settings. |
Example 2: Personal Preferences remain at customized setting after having been customized at some point.
| Condition | Language Settings | Comments |
|---|---|---|
| Default | System Language: English Personal Preferences: English |
This is assuming the software was installed as an English system. |
| Change Personal Preferences to French | System Language: English Personal Preferences: French |
The Personal Preferences have been customized. |
| Change Personal Preferences back to English | System Language: English Personal Preferences: English |
The settings are back to their defaults, but the Personal Preferences had been customized. |
| Change System Language to French | System Language: French Personal Preferences: English |
The Personal Preferences language settings no longer follow the System Language settings. |