Administer
This 
Use the links in the following table to find the content you are looking for.
| Function/Tool | Task | 
|---|---|
| Basic administration tasks | Run Updates, check database maintenance tasks. | 
| Cybersecurity | Provides recommended actions to help secure your system. | 
| Configuration Manager | Use Configuration Manager to back up the configuration on your system. (Note: This is an add-on tool. See Resources for information on where to get it.) | 
| Database Manager | Archive and trim the ION databases, upgrade a database, create a new database, or export the database registry settings. | 
| Deactivating alarms | Deactivate alarms that are incorrectly stuck in a permanently active state. | 
| Diagnostics Viewer | Monitor system and network performance. | 
| PME Installer | Reconfigure, reset accounts, export System Key, import System Key, uninstall. | 
| User Manager | Add or remove PME users. Change user access level, passwords, and account information. Change User Group access to devices and Web Applications. | 
| Windows Updates | Routinely apply Microsoft Windows Updates. |