Capacity Management Module operation
NOTE: This module requires a separate license. See Licensing for more information.
The Capacity Management Module provides generator, Uninterruptible Power Supply (UPS), and general equipment monitoring and reporting. It also includes transformer and UPS loss monitoring and reporting. The losses are reported in terms of energy and cost.
Use the Capacity Management Module to:
- Analyze IT branch circuit power loading.
- Understand remaining capacity at the branch circuit level.
- Understand generator and UPS system power loading.
- 
                                                Understand if the generator and UPS loading compromises the design redundancy of the backup supply system. 
The following reports are part of this module:
- Branch Circuit Power Report
- Equipment Capacity Report
- Generator Capacity Report
- Generator Power Report
- Power Losses Report
- UPS Power Report
For information on how use the Capacity Management Module reports, see Power Capacity Reports
Related topics:
Capacity Management Module topics
- Capacity Management Module Design
- Capacity Management Module configuration
- Capacity Management Module operation
Other Software Modules
- Backup Power Module operation
- Breaker Performance Module operation
- Energy Analysis Dashboard Module operation
- Energy Analysis Reports Module operation
- Energy Billing Module operation
- Event Notification Module operation
- Insulation Monitoring Module operation
- Power Quality Performance Module operation