Backup Power Module operation
NOTE: This module requires a separate license. See Licensing for more information.
The Backup Power Module provides generator and Uninterruptible Power Supply (UPS) monitoring and reporting. It reports on generator and UPS performance and battery health.
The Generator Test EPSS Report can be configured to conform to the requirements for an Emergency Power Supply System (EPSS) test, including automatic transfer switches (ATS). For example, the report shows the transfer time of the lead ATS and indicates whether the transfer time passes or does not pass the test requirements. See Emergency Power Supply Systems for more information on EPSS.
Use the Backup Power module to:
- Identify generator problems that could prevent a transfer to backup power.
- Automatically record and document the backup generator system test.
- Monitor the generator battery health.
- Report on backup generator run times.
- Monitor the condition of your UPS, including the battery health.
The following reports and diagrams are part of this module:
| Type | Reports | Diagrams | 
|---|---|---|
| Generator Performance | Generator Activity Generator Battery Health Generator Test EPSS Generator Load Summary | EPSS Diagrams | 
| UPS Performance | UPS Auto Test UPS Battery Health | UPS Auto Test diagrams | 
For information on how use the Backup Power diagrams and reports, see:
Related topics:
Backup Power Module topics
- Backup Power Module design
- Backup Power Module configuration
- Backup Power Module operation
Other Software Modules
- Breaker Performance Module operation
- Capacity Management Module operation
- Energy Analysis Dashboard Module operation
- Energy Analysis Reports Module operation
- Energy Billing Module operation
- Event Notification Module operation
- Insulation Monitoring Module operation
- Power Quality Performance Module operation