Using Table gadget in Slideshow

When you use the table gadget in slideshow, the slideshow in the new browser does not retrieve the real-time data from devices in the system. To retrieve the real-time data, perform the following:

  1. Open a new tab in the browser.
  2. Login to the PME web application.
  3. Refresh the slideshow page in the browser.

    The table gadget slideshow displays the real-time data from devices in the system.

NOTE: The session timeout of the PME web application is enabled by default (See Session Timeout for more information). After the timeout period, the slideshow display does not retrieve the real-time data. You must login to the PME web application every time after the timeout period.

Related topics:

Dashboards: