Applications
Use the information provided in this
Use the links in the following table to find the content you are looking for.
| Application | Description |
|---|---|
| Disturbance Direction Indicators |
This application (also known as DDD Indicators), can help you identify power quality disturbances, their type, and the likely location of origin. The disturbance information is shown with visual indicators that are integrated into an electrical one-line diagram. |
| Thermal Monitoring of Low Voltage (LV) Busways | This application provides continuous monitoring of the thermal conditions of low voltage busways. You can see temperature data in real-time, analyze historical temperature trends, and set up alarming based on temperature thresholds. |
| Thermal Monitoring of Medium Voltage (MV) Substations | This application provides remote, continuous monitoring of the thermal conditions of MV substations. You can see temperature data in real-time, analyze historical trends, and receive alarms and notifications. |