Design
Easergy CL110 or TH110 sensors, attached to the busway, wirelessly transmit real-time temperature measurements to a Harmony ZBRN32 access point. The access point is connected to PME through an Ethernet Gateway, such as the Link150. PME provides support for the access point, through an add-on Harmony ZBRN32 access point device driver.
After the access point has been configured in PME, the driver creates individual sources for each of the sensors that are connected to the access point. The driver also supports software logging of the temperature measurements. This is similar to how branch circuit monitors are handled in PME. One access point can support up to 60 temperature sensors.
The real-time and historical temperature data is available for display and processing in any of the relevant PME applications such as Dashboards, Diagrams, Trends, and Reports.
NOTE: The selection, installation, and configuration of the sensors, access point, and gateway is outside the scope of this application description. See Prerequisites for more information.