Guidance on choosing an architecture

There are a number of factors to consider when choosing whether to use Architecture 1, Architecture 2, or a combination of the two. The key factors to consider are:

NOTE: Hybrid versions of the architectures are possible, to meet specific application needs.