Computer hardware

PME

See Computer Hardware for information on hardware specifications.

Building Operation

For information on Building Operation hardware specifications, see the IT System Planning Guide - EcoStruxure Building Management.

PME and Building Operation on the same computer

CPU and RAM

As a general guideline, we recommend that you use the PME Advanced Systems hardware specifications for systems based on Architecture 2 where the PME and Building Operation software is installed on the same server.

HDD

To install PME and Building Operation on the same server, add 2 GB to the required PME HDD space for the Building Operation application and additional space for historical data in Building Operation.