Building Operation and PME version compatibility

The PME/EBO Integration solution supports the following software versions:

PME Version SBO 1.6 SBO 1.7 SBO 1.8 SBO 1.9 EBO 2.0 EBO 3.0.1 EBO 3.2.3 EBO 4.0.2 EBO 5.0 EBO
6.0.3
EBO
7.0.3
8.0 - - - - - - - -
8.1 - - - - - - - -
8.2 - - - - - - - -
9.0 - - - - - - - - -
2020 - - - - - - - - - -
2021 - - - - - - - - - -
2022 - - - - - - - - - -
2023 - - - - - - - - - -
2024 - - - - - - - - - -
2024 R3 - - - - - - - - - -

NOTE: Perform a refresh for the service to start pulling the real-time data in EBO, when a new device in added in PME via EWS (EcoStruxture WebService) to display the data correctly.

Operating Environment

PME

See Operating Environment for supported operating systems and SQL Server versions.

Building Operation

See IT System Planning Guide - EcoStruxure Building Management for supported operating systems and SQL Server versions.