Creating PME users for Building Operation
You need to create two different PME users for the integration with Building Operation:
- A user for the EWS connection between the two applications.
- A user for the Building Operation connection to the PME Web applications (Dashboards and Reports).
For information on how to create the EWS user, see Setting up EWS credentials.
For information on how to create the user to access the Web Applications, see "Adding a standard user" in the EcoStruxure™ Power Monitoring Expert System Guide or the PME Web Applications Help.