Recommended actions

PME is designed for a defense in depth security strategy, in compliance with IEC 62443, the global standard for industrial automation control system security. A defense in depth strategy is a multi-layered approach to cybersecurity with intentional redundancies to increase the security of a system as a whole.

The different defense in depth layers can be described as:

  • Data Layer (includes access control and encryption of data)
  • Application Layer (includes antivirus software and application hardening)
  • Host Layer (includes patch implementation, user authentication)
  • Network Layer (includes IPsec, intrusion detection system)
  • Perimeter Layer (includes firewalls, VPN)
  • Physical Layer (includes guards, switches, locks, ports, physical access)
  • Policies

To help secure your system, you must take specific actions for the different layers and at every stage of the project life-cycle. The following shows the actions we recommend to help secure your system, organized by life-cycle stage:

NOTE: The list of recommended actions below is not a complete list of possible cybersecurity measures. It is meant to be a starting point to improve the security of your system. Consult with cybersecurity experts to plan, install, configure, administer, and decommission your system based on your needs.

Life-cycle Stage Layer Recommended Action
Planning Data Layer Obtain security certificates.
Application Layer Obtain antivirus and application allowlisting software.
Host Layer Plan user access.
Network Layer Plan your network security.
Perimeter Layer Plan to install PME in an intranet environment.
Plan IP port use.
Physical Layer Plan your site security.
Policies Plan for the implementation of cybersecurity standards.
Installing, Upgrading Application Layer Install antivirus and application allowlisting software.
Verify install file integrity and authenticity.
Protect the System Key.
Apply PME updates.
Host Layer Install latest updates for OS and SQL Server.
Check computer for cybersecurity issues.
Network Layer Install your network security measures.
Configuring Data Layer Install security certificate.
Set up encrypted database communication for Distributed Database architectures
Application Layer Configure application allowlisting software.
Configure antivirus software on your SQL Server.
Host Layer Configure PME users and user groups.
Customize user account privileges.
Restrict Windows login permissions for the PME server.
Change the SQL Server Express sa account password.
Configure session timeout settings.
Do not install or use a web browser on the server computer.
Network Layer Set up your network security.
Perimeter Layer Disable unused IP ports.
Physical Layer Disable unused hardware ports.

Administering

Data Layer Renew security certificate.
Securely store the system key.
Application Layer Apply PME updates.
Verify update file integrity and authenticity.
Host Layer Apply OS updates.
Review user accounts on a regular basis.
Network Layer Keep network security up-to-date.
Physical Layer Keep computer hardware secure.
Policies Perform security audits
Decommissioning Host Layer Decommission your system at the end of its life.