Renew security certificate
Renew the security certificate before it expires.
Securely store the system key
See Protect the System Key for details.
Apply PME updates
Install software updates that apply to your system when they become available.
Verify update file integrity and authenticity
See Verify install file integrity and authenticity for details.
Apply OS updates
warning
potential compromise of System availability, integrity, and confidentiality
Apply the latest updates and hotfixes to your Operating System and software.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Critical and routine Windows updates can be applied to the operating systems hosting the PME server and clients without prior approval by
Consider implementing best practices, such as:
- Establish a reliable process for finding and applying the latest security updates.
- Use systematic procedures governed by corporate policy.
- Use automated scanners for detecting missing patches, misconfigurations use of default accounts, and so on.
warning
unintended equipment operation
| ● | Before installing the update, verify that the system is not performing critical control actions that may affect human or equipment safety. |
| ● | Verify correct system operation after the update. |
Failure to follow these instructions can result in death, serious injury, or equipment damage.
Apply SQL server and other components patch updates
warning
potential compromise of System availability, integrity, and confidentiality
Apply the latest updates and hotfixes to your SQL server and individual components shipped with PME.
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
warning
inaccurate data results
| ● | Before installing the update, verify that the system data results are not used for critical decision making that may affect human or equipment safety. |
| ● | Verify correct system data results after the update. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Critical and routine SQL Server other components patch updates can be applied to the operating systems hosting the PME server and clients without prior approval by
Consider implementing best practices, such as:
- Establish a reliable process for finding and applying the latest security updates.
- Use systematic procedures governed by corporate policy.
- Use automated scanners for detecting missing patches, misconfigurations, use of default accounts, and so on.
warning
unintended equipment operation
| ● | Before installing the update, verify that the system is not performing critical control actions that may affect human or equipment safety. |
| ● | Verify correct system operation after the update. |
Failure to follow these instructions can result in death, serious injury, or equipment damage.
warning
inaccurate data results
| ● | Before installing the update, verify that the system data results are not used for critical decision making that may affect human or equipment safety. |
| ● | Verify correct system data results after the update. |
Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.
Review user accounts on a regular basis
Review PME user accounts on a regular basis. Update passwords and user permissions, and remove unused accounts as required.
RECOMMENDATION: Use Windows users instead of standard users in your PME system to improve cybersecurity. Windows offers the advanced user management function of limiting the number of invalid login attempts. This function is required for IEC 62443 compliance, the global standard for industrial automation control system security.
NOTE: To only use Windows users, replace any existing standard users in the system with Windows users. Disallow logins for standard users in Web Applications, this disables the supervisor user.
Keep network security up-to-date
Keep security related networking tools and equipment up-to-date and working as expected.
NOTE: Network security equipment, such as firewalls, are complex devices and must be maintained by trained individuals.
Keep computer hardware secure
See Plan your site security for more information.
Perform security audits
Perform comprehensive system security audits on a regular basis. Regularly scan and verify security.
Consider implementing best practices, such as:
- Check the OS and PME system logs.
- Check performance monitor profiles