Installation process

The installation is a two-step process that must be performed in the following order:

  1. Installing the SQL Server.
  2. Installing the PME software.

 

NOTE: The same PME installer is used to install a Standalone Server, Application Server, or Engineering Client. Which component is installed is determined by the Setup Type, which you select during the installation. Based on this Setup Type, the installer displays the appropriate setup pages. See Setup Types and applicable Installer pages for more information.

For information on the different Setup Types, see Standalone Server, Application Server, Engineering Client.

Web Clients do not need to be installed. For information on Web Clients, see Client types.