Configure the Branch Circuit Power Report
CAUTION
inaccurate data results
● | Do not incorrectly configure the software or the devices. |
● | Do not base your maintenance or service actions solely on messages and information displayed by the software. |
● | Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements. |
Failure to follow these instructions can result in injury or equipment damage.
To configure the Branch Circuit Power Report:
- Set up the monitoring device that records the branch circuit data. See Supported measurements and devices for details on which measurements are required.
- Configure a hierarchy in PME using the
...\Power Monitoring Expert\applications\HierarchyManager\SampleTemplates\DataCenter\
template.
CustomerRackCircuitTemplate.xmlTIP: See Hierarchy Configuration Utility and Hierarchy Manager for information on how to install and maintain a hierarchy.
- Open the report template in the Reports Web Application, set the report input parameters, and generate the report.