UPS Power configuration restrictions
The UPS Power Configuration Utility enforces certain rules when you create UPS systems, groups, and modules:
- UPS System
- Name must be unique.
- One or more systems are allowed.
- UPS Groups
- Name must be unique.
- At least one group must be present in each system.
- A maximum of three groups are allowed in each system.
- For N, N+1, and N+2 system types:
- Each group in the system may have a different number of UPS modules.
- Each UPS module in the group must have the same nameplate rating (kVA) value.
- Each UPS module in the group must have the same derated nameplate rating (kW) value
- Each group is connected to one load only. No other group can be connected to the same load.
See the UPS Power Configuration Utility for more information.
- For 2N, 2(N+1) and 2(N+2) system types:
- All groups must have the same number of UPS modules.
- All UPS modules in the groups must have the same nameplate rating (kVA) value.
- All UPS modules in the groups must have the same derated nameplate rating (kW) value.
- Depending on the number of groups present in the system, a load may be shared by two groups.
See the UPS Power Configuration Utility for more information.
- UPS Modules
- Name must be unique.
- At least one module must be present in each group.
- A maximum of 12 modules is allowed in each group.
For information on UPS redundancy types, see UPS system redundancy types.