Setting a default Alarms view
The default Alarms view is the view that opens when you first open the Alarms application. You can set a default for your own workspace or the entire system.
NOTE: Access to this application or function is controlled by user privileges. 
To set a default Alarms view:
- In the alarm viewer, open the view library and navigate to the view you want to set as default.
 - Right-click the view name or click Options 
 for this view  and select Set as default. This opens the Configure Default Item dialog.  - In Configure Default Item, enable Set as my default or Set as system default.
 - Click OK to save the default settings.
 
Related topics:
- Adding a new Alarms view
 - Copying an Alarms view
 - Editing an Alarms view
 - Sharing an Alarms view
 - Moving an Alarms view
 - Deleting an Alarms view
 - Setting a default Alarms view
 - Changing the alarm viewer settings
 - Deactivating alarms
 
For reference information see:
For information on how to use Alarms, see Alarms.