Creating a processed measurement

Create processed measurement to duplicate the original measurement value and aggregate the new measurement value after the measurement value reaches the threshold or the associated device is replaced.

To create a processed measurement using the Device Replacement user interface:

  1. In Device Replacement, select the Processed Measurement tab, and then click Create.
  2. Select the Processed Measurement Name.

  3. (Optional) If you want to specify the processing start date, then turn off Start Processing from Beginning and select the date from the Processing Start Date.

  4. Click a measurement name in the Available Measurements area to select it.

    By default, the measurement names are listed in alphabetical order. You can use the Search field to find measurements by name.

  5. For a selected measurement, select the device in the Device Name area.

    By default, the device names are listed in alphabetical order. You can use the Search field to find devices by name.

  6. Click to select the device and measurement data series.

  7. (Optional) Perform step 4 to 6 for other measurements and devices.

  8. Click Add to list the selected measurement and device.

  9. Click Save.