Adding graphics pages
To add a new graphics page in the Graphics Editor:
- In PME, open the Graphics Editor.
- Double-click on each node to load the Managers, Modules, and Registers supported by each device type.
- From the left pane, drag and drop components to create the graphics page.
- To animate a component in the Graphics Viewer, in the Properties pane set up the component-specific Custom properties.
- To edit the Graphics Viewer menus, see the Defining the Graphics Viewer menu structure.
- Select Save.
- Select Validate TGML Document.
- In the Validate TGML Document window, view any binding issue details by component Type or Binding Notes. If there are error messages, correct the binding issues in the Graphics Editor workspace.
- To validate the TGML document, select Validate TGML Document in the toolbar.
The Graphic Editor loads and displays all the connected devices in the Binding pane.
NOTE: If any devices are added or deleted or renamed in Management Console or Device Manager, select Refresh Devices to view the latest device list.
NOTE: You can only open or save a file in the following path: ..\Program Files (x86)\Schneider Electric\Power Monitoring Expert\config\diagrams\tgml
If a binding property is incorrectly configured on any graphics page, a message appears and the Validate TGML Document window displays.