Data logs

When you need details about circuit measurements and details, the Area Details diagram provides links to the historical data log and the event log. These logs provide measurement data for the 5-minute polling interval of the LIM-IG6. You can filter the data in the logs by date range.

When using the event log, you can also generate a graph that shows THC measurements plotted across time. If any THC measurement exceeds the hazard threshold, the graph includes a callout at the specific event point.

Historical data log and graph

The following figure shows the historical log table.

The buttons located at the top of the table are:

  • Device Diagram – Click this to return to the diagram.
  • Change Date Range – Click this to view data for different dates. See "Select Date Range" below for more information.
  • Show Graph – Select one or more column headers in the table and click this to see a graph of the data. The graph shows the data at 5-minute intervals. For example, you can check the Total Hazard Current option in the table and see the values. Click a point on the data line to see details for that value, as shown next.

The following figure shows the historical log table from the Vista client view:

Event Log

The following figure shows the event log table:

The buttons located at the top of the table are:

  • Device Diagram – Click this to return to the diagram.
  • Change Date Range – Click this to view data for different dates. See "Select Date Range" below for more information.

Select date range:

For either type of log table, you can select the date range for data you want to see. The default date range is "Today".

  1. Click Select Date Range.

  2. Select an available range or click Between these dates and select specific dates in the calendar.
  3. Click Show Table to see the data.

If you select a date range of more than one week, a message appears to inform you that the table will be very long.

The new table appears.

See the following topics:

Different diagrams are provided for ANSI and IEC regulated applications:

Related topics:

For information on how to configure Diagrams, see Diagrams and graphics configuration.