Viewing user diagram of devices with security
You can view the user diagram of devices with security settings enabled in Diagrams application.
To view user diagram of the devices with standard security enabled:
- Log in to Web Applications with username and password.
- Navigate to Diagrams link.
The network diagram appears in the workspace containing icons that represent groups of devices on your system.
- Click Network Diagram.
- Click one of the grouping objects and display the node icons contained within.
- Click a node icon to display the user diagram for the associated device.
NOTE: To perform any control object function, enter the device password. The username is set to default. See Performing manual control actions for more information.
NOTE: You cannot view device data in the user diagram in Diagrams for devices with advanced security enabled. Control object functions for advanced security enabled devices are not supported in Diagrams.
Related topics:
- The Diagrams user interface
- User authentication
- Viewing historical (trend) data
- Viewing meter events
- Viewing user diagram of devices with security
- Performing manual control actions
- Stale data and error indicators
- Power Quality Performance diagrams
- Insulation Monitoring diagrams
- UPS Auto Test diagrams
- EPSS diagrams
- Breaker Aging diagrams
For information on how to configure Diagrams, see Diagrams and graphics configuration.