Event Notification Module operation
NOTE: This module requires a separate license. See Licensing for more information.
Use the Event Notification Module (ENM) to notify recipients about critical power system events. ENM can send notifications of power system events through email, SMS or SNMP. ENM uses the Alarms application to detect system events. You can set up notifications for activity in any of the event, alarm, or incident views. The notification details are defined in a notification rule. A notification rule can be enabled or disabled, and you can use a schedule to determine when the rule is applied. You can define more than one notification rule.
warning
unintended equipment operation
| ● | Do not rely solely on Event Notification Module use for alarm notification where human or equipment safety relies on the operation of the control action. |
| ● | Do not use Event Notification Module to control time-critical functions. |
| ● | Do not use the software to control remote equipment without proper access control and status feedback. |
| ● | Consider the implications of unanticipated transmission delays or failures of communications links. |
Failure to follow these instructions can result in death, serious injury, or equipment damage.
NOTE: Other parts of the overall communication system, such as email servers, cellular phone systems and SNMP servers, could fail and result in notifications not being delivered. If notifications are not delivered to recipients, conditions that cause alarming may persist and result in safety critical issues.
Notifications are sent out automatically based on the configuration of the module. See Event Notification Module configuration for information on how to configure notifications.
Related topics:
Event Notification Module topics
- Event Notification Module Design
- Event Notification Module configuration
- Event Notification Module operation
Other Software Modules
- Backup Power Module operation
- Breaker Performance Module operation
- Capacity Management Module operation
- Energy Analysis Dashboard Module operation
- Energy Analysis Reports Module operation
- Energy Billing Module operation
- Insulation Monitoring Module operation
- Power Quality Performance Module operation