Device Manager user interface
Main user interface (UI) and Devices tab
                                            
                                        
Main UI
| 1 | Selection tabs 
                                                         Select a tab to see information related to Devices or Sites.  | 
                                                
| 2 | 
                                                         Help
                                                              | 
                                                
| 10 | Number of displayed items
                                                         Shows the number of items visible on this page, and the total number in the system.  | 
                                                
| 11 | Page Selector
                                                         Use the page Selector to navigate between pages of information. Set the number of items that are displayed on a page.  | 
                                                
Devices tab
| 3 | 
                                                         Add Ethernet Device
                                                             NOTE: To add serial devices that are directly connected to the system, for example through a RS485 converter, or to add Logical Devices, use Management Console.  | 
                                                
| 4 | 
                                                         Import
                                                              | 
                                                
| 5 | Devices filter
                                                         Use the devices filter to customize which devices are displayed in the devices table. You can filter by Communication Status, Type, and Enabled State.  | 
                                                
| 6 | Search Devices box.
                                                         Enter a search string to find devices in the devices table.  | 
                                                
| 7 | 
                                                         Refresh
                                                             NOTE: The Communication Status indicator in the table is updated automatically every 10 seconds. To update the configuration information use Refresh.  | 
                                                
| 8 | 
                                                         Options menu
                                                              | 
                                                
| 9 | 
                                                         Devices table
                                                              | 
                                                
Sites tab
                                            
                                            
                                        
| 1 | 
                                                         Add Ethernet Gateway
                                                              | 
                                                
| 2 | 
                                                         Import
                                                              | 
                                                
| 3 | Sites filter
                                                         Use the sites filter to customize which sites are displayed in the sites table. You can filter by Communication Status, Type, and Enabled State.  | 
                                                
| 4 | Search Sites box.
                                                         Enter a search string to find sites in the sites table.  | 
                                                
| 5 | 
                                                         Refresh
                                                             NOTE: The Communication Status indicator in the table is updated automatically every 10 seconds. To update the configuration information use Refresh.  | 
                                                
| 6 | 
                                                         Options menu
                                                              | 
                                                
| 7 | 
                                                         Sites table
                                                              |