Importing network configuration from a different system
Import the device and site configuration that was exported from another system. For example, to create a copy of an existing system or to transfer the configuration from a test system into a production system. You can also import the configuration from configuration tools, such as ION Setup.
NOTE: You cannot import the configuration back into the same system from which it was exported.
To import the network configuration from a different system:
- In Device Manager, click Import. This opens the import wizard.
 - Follow the steps in the import wizard. Select the configuration file from the other system when prompted by the wizard to upload the import file.
 - Complete the configuration import in the import wizard.
 - Click Finish in the import wizard.
 
Related topics:
Devices
- Adding a device
 - Editing a device
 - Deleting a device
 - Connecting or disconnecting an Ethernet device
 - Enabling or disabling a device
 - Viewing a device diagram
 
Sites
- Adding a site
 - Editing a site
 - Deleting a site
 - Connecting or disconnecting a site
 - Enabling or disabling a site
 
Network
- Exporting network configuration for use in a different system
 - Importing network configuration from a different system
 
For reference information see: