Configure
This section describes the different tools and tasks for configuring Power Operation.
Use the links in the following table to find the content you are looking for:
| Section | Description | 
|---|---|
| Configuration prerequisites | Things to consider to help you prepare for configuring a Power Operation project. | 
| Changing configuration on a running system | Describes configuration changes that can be made on a running system. | 
| Configuration tools | An introduction to the Power Operation configuration tools. | 
| SCADA Projects | Creating a Power Operation project using Project Setup, and compiling, backing up, an restoring a project. | 
| Devices | Information and tasks on how to configure and work with: 
 | 
| Power Operation Runtime | How to configure and work with: 
 | 
| Web Applications | How to configure and work with: 
 | 
| Applications | Information on extending the capabilities of Power Operation by configuring applications. | 
| Managing user accounts, roles, and mapping | Configure and manage user access. | 
| Customize default behaviors | How to use Cicode to customize a project, localizing a project, and running PO as a Windows Service. | 
| System Startup and Validation Checks | How to validate your configured system on startup. | 
| Distributed systems | How to configure: 
 | 
| Redundant systems | How to configure a redundant server. | 
For more detailed resources on configuration, see the Configure references section.