Removing an I/O device from a project
To remove an I/O device:
- Open I/O Device Manager.
- Click Remove one I/O device, then click Next.
- At the Remove a device screen:
- Click the drop down menu to display the equipment names that were used when the device profiles were previously added to the project.
- From this list, select the device that you want to remove. Click Next.
- At the Ready to perform action screen:
- (Optional) Compress the project files after removing this profile, click Pack databases.
- Click Next.
After the device is deleted, a screen displays telling you that the project was updated successfully.
- To view a detailed list of the devices that you added or deleted, click View audit log. The list shows all the device data that was added, and the data that was removed in this session. (The list displays after you click Finish.)
- To remove additional devices, click Add/remove more devices, then click Next.
- Repeat steps 3 and 4.
- When you have finished removing devices, uncheck Add/remove more equipment, then click Finish.
If you clicked View audit, the list displays.
If you did not click Add/remove, the I/O Device Manager closes. If you clicked Add/remove, the Welcome screen displays again.
- Compile the project. Correct any compile errors and then compile the project again.