Profile Editor export
Export a Profile Editor project when you want to back up a Profile Editor project for re-use in another instance of the Profile Editor. This is useful when you have custom tags and custom devices that you want to share in other projects. After you export a project, you can import it to another Profile Editor project.
To back up a project file, see Backing up a project.
To export a Profile Editor project:
- In Profile Editor, select the Set Up Projects tab.
- From the Project drop down box, select the project you want to export.
- Select File > Export > Profile Editor Export.
- See Customize tag names and Add project parameters for the information you need to make the changes that you want.
- Select Export Project.
In addition to the project data, exported projects include:
- A unique project name, the date of the export
- The name of the computer to which it was saved
- (Optional) The description added when the source project was created.
The project – which will be named YOUR PROJECT.pls – is exported to the following location:
[Project Drive]\ProgramData\Schneider Electric\Power Operation\v2022\Applications\Profile Editor\Projects\YourProjectName.pls