Exporting configuration packages
In Profile Studio, check your project for errors and completeness prior to export.
Validate a project
- In the main menu, select the Validate configuration button.

The Check errors tab appears in the Main View pane if errors are found.
A completed project can contain:
- Assigned profiles that exist.
- Datapoints that exist, are associated with profiles, have unique descriptions.
- SignalList, a CSV file containing all datapoints, device links, or virtual datapoints.
- Device links that exist, are associated with profiles, have unique descriptions.
- Virtual datapoints that exist, are associated with profiles, have unique descriptions.
- Virtual datapoints with inputs that exist.
After configuration, export a configuration package in the form of a ZIP file.
|
HMI used |
Package contains: |
|
EcoSUI |
|
|
EcoGTW |
|
|
Power Operation |
|
You can export a configuration package for all equipment, or a configuration package for selected equipment only.
Export modified configuration packages
- In the main menu, select the Export configuration full package button.

If one or more of your exported datapoints share the same description, the SCL export options dialog appears. Enable or disable the following options: - Ignore check errors: Enable to ignore errors found during validation.
- Spare duplicate description: Enable to exclude the duplicate description(s).
- Rename duplicate description: Enable to rename the duplicate description(s).
- Select OK.
- Select a location for your finished package.
Your ZIP is exported to the selected location.
Export selected configuration packages
You can import your configuration package into Power Operation Studio by loading it into the I/O Device Manager. Modified IHMIs are exported.
- In the Equipment tab, select the IHMIs you wish to export by right-clicking the device name. Hold down CTRL to select multiple devices.
- Choose Export equipment configuration package from the context menu.
- Select a location for your finished package.
Your ZIP(s) are exported to the selected location.
See Devices for information about importing devices from a CSV file.
Before importing into Power Operation Studio, you will need to open your CSV file and add the absolute path of the SCD file to the PrimarySclFileName column. You also have the option of modifying the Cluster and Primary IO Server Name columns at the same time. See Create a CSV file to add multiple devices for more information about the columns in your CSV file.